Select Your Country

Go to global website

8-Inch Tab-Ex® 05 Tablet Sets New Standards in 5G Communication

Tab-Ex® 05 Tablet DZ1 and DZ2 version

Digitalized workflows are increasingly finding their way into the (process) industry. Mobile devices such as smartphones and tablets used in these fields have to meet the latest safety standards and be reliable and convenient to operate even in the most adverse environmental conditions.

With the new Tab-Ex® 05, Pepperl+Fuchs is launching the first 5G-capable Android tablet with an 8-inch screen that is approved for use in Zone 1/21 and Div. 1. The Android Enterprise Recommended device is based on the Samsung Galaxy Tab Active5 and comes with a range of sophisticated features.

Powerful Without Compromise

The Tab-Ex 05 has 6 GB RAM and 128 GB ROM, which can be expanded to up to 1 TB via microSD. It is also equipped with a 13 MP camera on the back and a 5 MP camera on the front, which deliver high-resolution imageand video recordings. Like its predecessor models, the Tab-Ex 05 features an individually programmable button that can be assigned to emergency calls or push-to-talk applications, for example. The S Pen Stylus pen with a fine 0.7 mm tip complements the user-friendly operating concept and allows handwritten notes to be taken or digital signatures to be captured on the move.

Certified for Global Use

The most recent addition to the Tab-Ex series complies with the latest European and international standards and meets approvals for global use. The basic Samsung Galaxy Tab Active5 device also has the internationally recognized Common Criteria security certification. Guaranteed operating system updates up to Android 22 and security updates up to 2032 offer companies a high degree of future security when it comes to selecting tablet solutions for long-term global use in industrial applications and hazardous areas.

Due to the wet touch function and IP68 degree of protection, the tablet is protected against the ingress of water and enables smooth operation in rain and snow. Even in outdoor areas of industrial plants, the device can be operated comfortably and without restrictions in glove mode. Biometric authentication technologies are also a particular advantage: state-of-the-art facial recognition functions ensure maximum security and user-friendliness.

AR Technologies as an Efficiency Booster

Mobile worker using the Tab-Ex 05 for maintenance

The Tab-Ex 05 really shows its strengths in complex applications based on augmented reality (AR). The tablet has an AR-capable camera and an extended set of tracking tools—including an accelerometer, a gyroscope, a GPS module, and a geomagnetic sensor. This enables location-based AR functions such as indoor localization, which makes working in hazardous areas even safer. Due to Google ARCore certification, the Tab-Ex 05 is ideally suited for remote support, training, and the use of company-specific tools. This makes the tablet an efficient companion in a wide range of industrial applications, from administration to predictive maintenance of systems.

Users can flexibly decide at any time whether they want to use the tablet on the move or in the office in wireless DeX mode (desktop mode) with a larger screen, creating a fully-fledged and cost-saving alternative to stationary desktop PCs.

Highlights of the Tab-Ex 05

  • Continuation of the successful 8-inch Tab-Ex tablet series with 5G support for hazardous areas
  • Based on the Samsung Galaxy Tab Active5, the Tab-Ex 05 offers reliable use and operation even in challenging environmental conditions
  • Android updates up to Android 22 and security updates up to 2032 guarantee long-term usability
  • Augmented reality functions such as indoor localization ensure safer and more efficient work in hazardous areas

More Information