物流行業中智慧感測器的解決方案
物流行業中智慧感測器的解決方案
无论是自动存储和检索系统、输送系统、自动导引车辆(AGV)、工业车辆还是起重机,倍加福传感器能够适用于物流行业中的各种应用。点击观看优酷视频,了解倍加福解决方案如何实现可靠防撞、安全导航或位置检测。
The G20 48V motor control module was designed for modern, complex conveyor systems. The modules offer higher performance with the same power consumption. This means that fewer power supplies need to be installed along the conveyor line, making system planning much more flexible ... Learn more
为了检测输送线上不同类型的托盘,倍加福开发了一种模块化传感器解决方案:托盘检测器是由一个专为应用设计的传感器支架与光电或超声波传感器结合组成,具体取决于托盘类型 ... 了解更多
倍加福为监控传送带占用率提供了高效的解决方案:Contour2D 传感器系统只需要一个 LiDAR 传感器,可以快速轻松地调试 … … 了解更多
装载、固定和运输货物等多项任务为自动引导车辆AGV的应用带来许多挑战。倍加福提供了丰富的,紧凑而坚固的传感器产品组合,适用于从对接到负载定位和检测,再到负载识别等自动引导车辆应用 … 了解更多
为了在物流运输中实现高吞吐量,自动导引车辆(AGV)必须在各种情况下都能确保可靠导航。无论是自由导航、基于地面标签的导航还是运动跟踪,倍加福都提供了强大、先进的技术,以实现精确的导航引导 ... 了解更多
Whether in logistics centers, on factory premises, or in office buildings—AGVs must accurately detect their surroundings at all times to rule out collisions with people and objects. Pepperl+Fuchs offers sensors and systems for reliable environment perception, ensuring smooth operations ... Learn more
In factories and warehouses, the speed of an industrial truck must be restricted more than in outdoor areas. This is ensured by a vertically aligned radar sensor mounted on the roof of the vehicle. As soon as an indoor area is reached, the sensor detects the hall ceiling, so that the speed can be reduced automatically ... Learn more
In order to pick up and place pallets safely, the exact position of the fork needs to be determined. The ECA10TL cable-pull rotary encoder detects the height position with maximum precision. The rotary encoder is mounted on the industrial truck, while the cable eye is attached to the moving fork ... Learn more
For safety reasons, it must be reliably detected whether the driver of an industrial truck is in the correct position on the driver's seat. Ultrasonic sensors ensure interference-free driver detection, regardless of ambient conditions and optical properties ... Learn more
The IMU F99 inertial measurement unit is the ideal solution for detecting the inclination of the mast and leveling the industrial truck accordingly. The combination of acceleration sensor, gyroscope, and intelligent sensor fusion algorithm provides reliable measurement results even when the truck is in motion ... Learn more
Radar sensors offer a simple and wear-free solution for determining the lift height of forks: mounted on the fork carriage, they measure the distance to the ground so that no additional target is required. Due to the CANopen interface, the sensors are ideal for integration into industrial trucks ... Learn more
Defective pallets can lead to collisions during automatic compartment assignment in high-bay warehouses, causing major property damage. Due to its stable scanning axis in combination with a high angular resolution, the R2000 Detection reliably detects even small fragments of broken pallets … Learn more
配备堆垛机的自动化高架仓库为了加强吞吐量,同时避免故障和停机。将工业视觉相机直接安装在堆垛机上,监控其存储和检索的过程,以便员工在发生故障时能够立即采取行动 … 了解更多
堆垛机需要垂直和水平定位,以及毫米级的测量精度。R1000 测距传感器非常适合这项艰巨的任务:采用脉冲测距技术(PRT),可以实现高精度距离测量,确保精确定位 ... 了解更多
光通訊設備確保與堆垛機或穿梭車進行雙向乙太網通信。LS682光通訊具有恒定的傳輸速率,可在300米的距離內實現穩定的連接。完全無磨損,保證通訊的平穩流暢…… 了解更多
R10X系列光電感測器在同樣的一個緊湊的外殼中,通過結合不同的光學功能,可以輕鬆適應各種特定的應用需求。具有背景抑制功能的漫反射型感測器是用於倉位檢測的理想之選…… 了解更多
Due to multiple code redundancy, the PXV positioning system is a particularly reliable solution for positioning automated storage and retrieval machines. If safe positioning is required, safety variants in accordance with SIL 3/PL e are also available ... Learn more
Space for the integration of sensors is often limited in shuttle storage systems. With its compact design, the R200 distance sensor with Pulse Ranging Technology even fits into small automatic shuttles. The tasks range from checking shelf occupancy and the correct load position to distance measurement and collision avoidance ... Learn more
To protect man and machine, strict safety requirements have to be observed when positioning storage and retrieval shuttles. The safePXV positioning system enables safe linear absolute positioning in accordance with SIL 3/PL e, using only a single sensor ... Learn more
The PHA vision sensor is ideal for the precise positioning of stacker cranes in high-bay warehouses. The sensor only requires a drill hole in the steel profile of the storage frame as a reference point, so no additional aids such as reflectors are necessary ... Learn more
In container ports, different crane types ensure efficient loading of containers. The position encoding system (WCS) records the position of cranes and trolleys with millimeter precision. With an outdoor protective housing and a stainless-steel code rail, the WCS can be used in harsh environmental conditions. For safety applications up to SIL 3/PL e, the system can be combined with the safe evaluation unit (PUS) ... Learn more
The robust incremental rotary encoders of the ENI90 series guarantee high-precision speed control due to integrated BlueBeam technology. Heavy-duty and offshore versions withstand the most adverse environmental conditions, which makes them ideal for monitoring crane drives in outdoor areas ... Learn more
With mobile cranes, the extension and retraction movements of the boom must be recorded in real time. This task is performed by the ECN40HD cable-pull rotary encoder, which can even be used in offshore applications due to its heavy-duty design. The open cable pull system enables easy cleaning and facilitates handling ... Learn more
由於RFID系統抗污垢、抗灰塵,以及具有不同的頻率範圍(低頻,高頻,超高頻),因此可適用於各種不同的應用領域。無論是揀選貨物還是在最終的汽車裝配過程中,通過提高透明度,RFID系統能減少管理錯誤並提高流程效率…… 了解更多
倍加福新型 RFID 门禁解决方案,可在检测大量 RFID 标签时实现无缝连接及过程透明化。该系统十分经济高效,以功能强大、标准化的 UHF RFID 技术为基础,并针对物流应用进行了专业优化,如跟踪货物的进出库… 了解更多
光學識別系統可輕鬆適應不同的應用,即使在複雜的環境條件下也能可靠地檢測物體 —— 如高速或高溫的應用中…… 了解更多
若您對我們提供的物流行業中智慧感測器的解決方案有任何疑問,請直接聯繫我們。
我們十分樂意為您提供幫助!只需填寫下表的資訊,發送電子郵件或預約,即可獲得您感興趣的產品的更多資訊。